Technical FAQs

Ask a Question

Unable to connect to an ION7700 meter using ION setup

When using ION Setup to connect to an ION7700 meter, the meter must be configured to use ION Protocol. If the meter is set to Modbus, ION Setup will be unable to connect to it.


Legacy KB System (APS) Data: RESL211138 V1.0, Originally authored by MaTh on 04/06/2013, Last Edited by MaTh on 04/06/2013
Related ranges: ION7700
Was this helpful?
What can we do to improve the information ?