Technical FAQs

Ask a Question

Which ION Module Outputs can be written to?

Below is a list of all the ION modules that accept a write to their output register:
1. External Boolean > Switch
2. External Pulse > Numeric
3. External Numeric > Trigger
4. Integrator module > Result
5. Diagnostic module > Battery Remaining (meter has to be in Test mode)


Legacy KB System (APS) Data: RESL211094 V1.0, Originally authored by MaTh on 03/30/2013, Last Edited by MaTh on 03/30/2013
Related ranges: Power Monitoring 7.0, ION Enterprise V6.0
Was this helpful?
What can we do to improve the information ?