Technical FAQs

Ask a Question

Is the BCPM Supported on the Sub-Meter Display (SMD)?

Product Line:
Branch Circuit Power Meter (BCPM)

Firmware upgrade

*Warning: The firmware utilities listed here can cause permanent damage to your product if applied incorrectly. Before downloading any firmware updates, verify the firmware you are downloading is appropriate for the specific model number of your product. If you have any doubts, contact Technical Support for guidance. 

*Warning: Devices should be disconnected from all monitoring software before performing a firmware upgrade*

The BCPM is supported on the sub-meter displays with firmware version of 25 or higher. If the SMD is not at firmware version 25, the firmware can be upgraded using the DLF-3000 firmware utility. Below the utility, firmware, and directions can be downloaded.

Use the following link to download the DLF-3000 software:
DLF-3000 Download

Was this helpful?
What can we do to improve the information ?