Technical FAQs

Ask a Question

Is it possible to sort a System Manager Software (SMS) Default Reports report?

Goals and Symptoms

Issue
User wants to sort a SMS Default Reports report such as "System Device Grouping Summary"

Causes and Fixes

Procedure

1. Open the System Device Grouping Summary Report from in the SMS Setup Utility by clicking on Reports/System Reports.
2. Find the System Device Grouping Summary as shown below and click on Preview Report.



3. Right click and Export to Excel. Excel will allow sorting. Note: Microsoft Office is required for this functionality.


Legacy KB System (APS) Data: RESL211061 V1.0, Originally authored by MaTh on 03/27/2013, Last Edited by MaTh on 03/27/2013
Related ranges: System Manager 4.3, System Manager 4.2, System Manager 4.0
Was this helpful?
What can we do to improve the information ?