Technical FAQs

Ask a Question

What is the refresh rate of measured quantities displayed on the EM3500 Series LCD display?

Goals and Symptoms

Issue
What is the refresh rate of measured quantities displayed on the EM3500 Series LCD display?

Causes and Fixes

Resolution

The PowerLogic EM3500 models calculate and update measurements once per second. This applies to both the values being displayed on the LCD and values in the Modbus point map and BACnet data objects. The update rate is not configurable.


Legacy KB System (APS) Data: RESL211059 V1.0, Originally authored by MaTh on 03/27/2013, Last Edited by MaTh on 03/27/2013
Related ranges: EM3500 series
Was this helpful?
What can we do to improve the information ?