Technical FAQs

Ask a Question

What are prohibited characters when naming a device or group in ION Enterprise or StruxureWare Power Monitoring?

IONE and SPM Naming Convention:
The Device Group and Name cannot contain spaces or the following characters:

\ / : * ? " < > { } . , ' & @ | %


A computer name can be up to 15 alphanumeric characters with no blank spaces, and it must
not contain any prohibited characters such as:
\ * + = | : ; < > ? , _
For compatibility with StruxureWare Power Monitoring software, use only letters and
numbers, starting the name with a letter for the first character in the name.


Legacy KB System (APS) Data: RESL211054 V1.0, Originally authored by MaTh on 03/27/2013, Last Edited by MaTh on 03/27/2013
Related ranges: Power Monitoring 7.0, ION Enterprise V6.0, ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?