Technical FAQs

Ask a Question

How to add the EM4800, ION, Powerlogic, and third party devices that are not supported natively in TMSCE 2.5 and are connected to an EGX300

In order to add the EM4800, ION, Powerlogic, and third party devices that are connected to an EGX300 the FTU (File Transfer Utility) needs to be installed and the FTP site has to be created. To do so follow the instructions in the attached file called "Powerlogic File transfer Utility Installation Guide"
PowerLogic File Transfer Utility Installation Guide.pdfPowerLogic File Transfer Utility.zip


Legacy KB System (APS) Data: RESL211050 V1.0, Originally authored by MaTh on 03/26/2013, Last Edited by MaTh on 03/26/2013
Related ranges: Tenant Metering Software
Was this helpful?
What can we do to improve the information ?