Technical FAQs

Ask a Question

How to import archived Advanced Reports data into the Advanced Reports database

Issue
How to import archived Advanced Reports data into the Advanced Reports database

Product Line
SMS 4.x

Environment
Archive database import

Cause
User wishes to import archived Advanced Reports data back into the live Advanced Report database. 

Resolution
1. Open the SMS Setup utility then go to Setup/Administrative/Advanced Reports/Database Maintenance.






2. Click on the Import Data tab and then browse for the archive file which needs to be imported.




3. After opening the archive file, click on Import.
4. The data is now in the live Adanced Reports database for reporting purposes. 

Was this helpful?
What can we do to improve the information ?