Technical FAQs

Ask a Question

How are Alarm Positions mapped in Event Notification Module (ENM) Alarm Sentry for PowerLogic CM4000s, CM3000s and PM800s?

Goals and Symptoms

Issue
When mapping a alarm position in ENM's Alarm Sentry, it is not possible to determine how the alarm position relates to the alarm number onboard the meter.

Causes and Fixes

Resolution

The below is a map corresponding to the onboard alarm number and the alarm position number in ENM:

CM4 and CM3





PM8





Legacy KB System (APS) Data: RESL210998 V1.0, Originally authored by MaTh on 03/20/2013, Last Edited by MaTh on 03/20/2013
Related ranges: Paging Module, PM800 series, CM4000 series, CM3000 series
Was this helpful?
What can we do to improve the information ?