Technical FAQs

Ask a Question

How to reset the ITIC/CBEMA web page graph in the ECC21

The ITIC/SEMI web page is based on the disturbance event log. To reset this log, write to the following to registers of the host meter using either Modbus Tester, SMS or ION Setup 3.0 or later.

Register Value
8000 4210
8001 1

Legacy KB System (APS) Data: RESL210986 V1.0, Originally authored by MaTh on 03/18/2013, Last Edited by MaTh on 03/18/2013
Related ranges: ECC21
Was this helpful?
What can we do to improve the information ?