Technical FAQs

Ask a Question

Why does the High Speed Power Meter Module show only whole numbers for an ION 7600 meter?

The ION 7600 meter has been designed to show only whole numbers (no decimal points) when using the high speed power meter module. If higher resolution (decimal points) is needed use the "regular" power meter module.


Legacy KB System (APS) Data: RESL210955 V1.0, Originally authored by MaTh on 03/13/2013, Last Edited by MaTh on 03/13/2013
Related ranges: ION7500/ION7600
Was this helpful?
What can we do to improve the information ?