Technical FAQs

Ask a Question

Is there a way to save and export the configuration file from an EGX300 to another EGX300?

Goals and Symptoms

Issue
Is there a way to save and export the configuration file from an EGX300 to another EGX300?

Facts and Changes

Copy EGX configuration

Causes and Fixes

Resolution

The .cfg file can be accessed via FTP and copied to another EGX300. Please see the attached pdf for instructions.

EGX300_CopyConfiguration.pdf


Legacy KB System (APS) Data: RESL210954 V2.0, Originally authored by MaTh on 03/13/2013, Last Edited by MaTh on 03/21/2013
Related ranges: EGX300
Was this helpful?
What can we do to improve the information ?