Technical FAQs

Ask a Question

Can the EM4800 communicate BACnet and Modbus TCP simultaneously over ethernet?

Issue
Can the EM4800 communicate simulataneously BACnet and Modbus TCP/IP over Ethernet?

Product Line
EM4800 series

Environment
Communication

Cause
EM4800 series meters only have one Ethernet port and no other form of communication.

Resolution
Yes, the EM4800 series can communicate over BACnet and Modbus TCP/IP over its Ethernet port simultaneously.
 
Was this helpful?
What can we do to improve the information ?