Technical FAQs

Ask a Question

Where is "Update Period" in StruxureWare Power Monioring 7?

Goals and Symptoms

Issue
Within the advanced device properties of Management Console for ION Enterprise version 5.5 there is an "Update Period" option which is the interval between requests to the device.



This option is configured on a device by device basis and it may be desirable to increase the value if one or more devices is experiencing intermittent communications.

Facts and Changes

Environment

StruxureWare Power Monitoring 7 (SPM 7, SPM7)

Causes and Fixes

Resolution

This same option has been moved to Vista within SPM7 and can be accessed by right clicking in the white space on the background and selecting the properties option.


The default settings will appear as below:



This is a global setting.


Legacy KB System (APS) Data: RESL210829 V1.0, Originally authored by MaTh on 03/01/2013, Last Edited by MaTh on 03/01/2013
Related ranges: Power Monitoring 7.0
Was this helpful?
What can we do to improve the information ?