Technical FAQs

Ask a Question

When running a report on an achive database in Web Reporter in ION Enterprise 6, the user receives an error message stating "An error occurred while generating a report, please consult the management console error log for more details"

This is caused by applying service pack 1 to an ION Enterprise 6.0 system and not updating the archives. To update the archives, open the database manager from within the management console, right click on databases and select upgrade databases. You will have to upgrade one archive at a time.


Legacy KB System (APS) Data: RESL210827 V1.0, Originally authored by MaTh on 03/01/2013, Last Edited by MaTh on 03/01/2013
Related ranges: ION Enterprise V6.0
Was this helpful?
What can we do to improve the information ?