Technical FAQs

Ask a Question

Is it possible to run a report on multiple archives at the same time with ION Enterprise?

Yes, the report must be ran using Report Generator. Web Reporter does not have the capability to run a report on multiple archives. To open the report generator click Start > Run > type in repgen and hit enter.


Legacy KB System (APS) Data: RESL210824 V1.0, Originally authored by MaTh on 03/01/2013, Last Edited by MaTh on 03/01/2013
Related ranges: Power Monitoring 7.0, ION Enterprise V6.0
Was this helpful?
What can we do to improve the information ?