Technical FAQs

Ask a Question

What is the HTML refresh rate of the default webpages included with the ION7600/7500 series Webmeter?

Product Line
ION7600/7500

Environment
Webpage

Resolution
By default, the webpages are static and require a manual refresh. However, custom webpages can be created using the Web Page Module of the meter in which the "HTML Refresh Rate" setup register will be passed along to the browser. Therefore, you can modify this setting by creating a custom web page and changing the refresh rate from it's default of 0 (no refresh) to the desired value.

Was this helpful?
What can we do to improve the information ?