Technical FAQs

Ask a Question

How many custom devices and custom quantities per device does the EGX300 support?

The EGX300 can support 10 custom device templates.
For each device template, a maximum of 120 quantities can be added.


Legacy KB System (APS) Data: RESL210393 V1.0, Originally authored by MaTh on 01/22/2013, Last Edited by MaTh on 01/22/2013
Related ranges: EGX300, Ethernet and TCP/IP
Was this helpful?
What can we do to improve the information ?