Technical FAQs

Ask a Question

The background image is not displayed in Diagrams (WebReach)

Goals and Symptoms

Issue
In StruxureWare Power Monitoring, the background image is not being displayed in Diagrams (formly known as WebReach). Vista is showing the background image correctly.

Facts and Changes

Environment

SPM 7.0.1, SPM 7

Causes and Fixes

Cause

This is possible if the image file name has "&" in it. E.g. the file name is "R&D Device.bmp".


Resolution

The workaround is to rename the background file and remove the "&" symbol. e.g. "RandD_Device.bmp".


Legacy KB System (APS) Data: RESL210390 V1.0, Originally authored by MaTh on 01/22/2013, Last Edited by MaTh on 01/22/2013
Related ranges: Power Monitoring 7.0
Was this helpful?
What can we do to improve the information ?