Technical FAQs

Ask a Question

Event Notification Module (ENM) Object Error when selecting "Relay Name"

Goals and Symptoms

Issue
When a user selects "Relay Name" in the "Relay & Recipient" tab, a yellow triangle will show beside "Relay Name" and a description of a Object Error. ENM will not allow the user to proceed.

Facts and Changes

Environment

Event Notification Module 7.0

Causes and Fixes

Cause

ENM 7.0 is not compatible with IE9.


Resolution

Downgrade to IE8 and make sure to use IE8 in compatibility mode.

If Internet Explorer 9 has been installed by Windows Updates, then it can be removed by going to Control Panel\Programs and Features\Installed Updates


Legacy KB System (APS) Data: RESL210386 V1.0, Originally authored by MaTh on 01/22/2013, Last Edited by MaTh on 01/22/2013
Related ranges: Paging Module
Was this helpful?
What can we do to improve the information ?