Technical FAQs

Ask a Question

Which I/O point numbers correspond to the physical I/O's from the different PM8 (PM800) option modules?

Issue
A user can not find the I/O point numbers that correspond to the I/O for the options module cards.

Product Line
PM800 Series Meter

Environment
PM800 series meter with I/O options module 

Cause
It may be difficult to determine the I/O point number for an I/O based on the I/O point, Option Module, and location of the Option Module.

Resolution
The following table displays the I/O point numbers for I/O on a PM800 with any options module.


The attached Excel file can be used to filter the I/O points and corresponding Modbus registers based on the I/O point, Option Module, and location of the Option Module.
 

Legacy KB System (APS) Data: RESL210332 V1.0, Originally authored by MaTh on 01/15/2013, Last Edited by MaTh on 01/15/2013
Related ranges: PM800 series
Was this helpful?
What can we do to improve the information ?