Technical FAQs

Ask a Question

ION desktop shortcuts were deleted. What are the path locations to recreate?

Goals and Symptoms

Issue
ION/SPM shortcuts were deleted by the user.

Causes and Fixes

Resolution

To create new shortcuts, navigate to the install path, right click on the file and click 'create shortcut'. The shortcut can then be copied to the desired location (e.g. Desktop).

ION Taskpad
Install Path\Schneider Electric\ION Enterprise\system\bin\ION Taskpad.exe
Designer
Install Path\Schneider Electric\ION Enterprise\system\bin\designer.exe
Vista
Install Path\Schneider Electric\ION Enterprise\system\bin\vista.exe
Web Reporter
Install Path\Schneider Electric\ION Enterprise\system\bin\IONWebLauncher.exe
Management Console
Install Path\Schneider Electric\ION Enterprise\system\bin\managementconsole.exe


Legacy KB System (APS) Data: RESL210198 V1.0, Originally authored by MaTh on 01/03/2013, Last Edited by MaTh on 01/03/2013
Related ranges: Power Monitoring 7.0, ION Enterprise V6.0
Was this helpful?
What can we do to improve the information ?