Technical FAQs

Ask a Question

Does ION Enterprise 6 or Struxureware Power Monitoring 7 record the BCPM energy readings for each individual circuit and can a tabular report be run on an individual circuit?

ION Enterprise 6 and Struxureware Power Monitoring (SPM) 7 will both record kwh del-rec automatically for an individual circuit for BCPM Model A. Individual circuit reports can then be run.
Note: BCPM B and BCPM C do not record energy values.


Legacy KB System (APS) Data: RESL210193 V1.0, Originally authored by MaTh on 01/03/2013, Last Edited by MaTh on 01/03/2013
Related ranges: BCPM(Branch Circuit Power Meter)
Was this helpful?
What can we do to improve the information ?