Technical FAQs

Ask a Question

Error during "Attach SQL Server Databases" portion of StruxureWare Power Monitoring 7.0.1 Install

Goals and Symptoms

Issue
During the SPM 7.0.1 install the installer stops on the step Attach SQL Server Databases with the following error:

Request Name: ConfigureSQLDBs
Information: Request ConfigureSQLDBs fail at function call:AttachDatabaseWithName

Facts and Changes

Environment

SPM 7, SPM 7.0.1 Install

Causes and Fixes

Cause

When the user installed SQL, the user account specified was not the Local System account and did not have local permissions.


Resolution

Re-configure the SQL Server Services to use either use the Local System account or an account with local permissions.


Legacy KB System (APS) Data: RESL210091 V1.0, Originally authored by MaTh on 12/19/2012, Last Edited by MaTh on 12/19/2012
Related ranges: Power Monitoring 7.0
Was this helpful?
What can we do to improve the information ?