Technical FAQs

Ask a Question

Is SQL Reporting Services required for ION 5.6?

SQL Reporting Services is used for the web based reporting engine in ION 6 and SPM 7. It is not required for a ION 5.6 installation.


Legacy KB System (APS) Data: RESL210077 V1.0, Originally authored by MaTh on 12/18/2012, Last Edited by MaTh on 12/18/2012
Related ranges: ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?