Technical FAQs

Ask a Question

Error during "Creating ION Enterprise Stored Procedures" portion of Event Notification Module (ENM) install

Goals and Symptoms

Issue
The ENM install is failing on step: Creating ION Enterprise stored procedure

Request Name: CreateIONStoredProc
Information: Error setting connection string



The following error is listed in the install log:

 
        • <?xml version="1.0" encoding="utf-16"?>
          <Attached>
          <SetIONConnectionString
          Library="InstallTools.Extensions.eSolutions"
          Class="SchneiderElectric.Installer.InstallTools.Extensions.eSolutions.ConfigureIONSQL"
          UIMessageOnFail="Error setting connection string.">
          <ionDbRegKeys>SOFTWARE\Schneider Electric\ION Enterprise\7.0.1\Databases|SOFTWARE\Schneider Electric\ION Enterprise\7.0\Databases|SOFTWARE\Schneider Electric\ION Enterprise\6.0\Databases</ionDbRegKeys>
          <ionRegistryView>Registry32</ionRegistryView>
          <enmRegistryPath>SOFTWARE\Schneider-Electric\PowerLogic eSolutions\SPM</enmRegistryPath>
          </SetIONConnectionString>
          </Attached>


Upon further investigation, the following message is displayed in the install log:

An error occurred while determining IONE database connection. Exception: Could not find file 'PorductInfo.xml' at any of ...

Facts and Changes

Environment

Distributed ENM install (is likely to occur on non-distributed installs)

Causes and Fixes

Cause

Install is from a network share (mapped drive)


Resolution

The customer should install ENM either from the DVD or from a local disk. Installing from a mapped/remote location can cause errors.


Legacy KB System (APS) Data: RESL210027 V1.0, Originally authored by MaTh on 12/14/2012, Last Edited by MaTh on 12/14/2012
Related ranges: Paging Module
Was this helpful?
What can we do to improve the information ?