Technical FAQs

Ask a Question

What settings are copied from each source device to target devices using the Multi Setup feature in SMS from Devices Routing?

Goals and Symptoms

Issue
What settings are copied from each source device to target devices using the Multi Setup (multiple device setup) feature in SMS from Devices Routing?

Facts and Changes

Environment

Any version of System Manager Software (SMS)

Causes and Fixes

Cause

User wants to copy device settings from one device to another

Resolution


Make sure the Enable Alarms on Destination box is checked as shown below


Legacy KB System (APS) Data: RESL209968 V1.0, Originally authored by MaTh on 12/11/2012, Last Edited by MaTh on 12/11/2012
Related ranges: System Manager 4.3, System Manager 4.2, System Manager 4.0
Was this helpful?
What can we do to improve the information ?