Technical FAQs

Ask a Question

How to configure a KWh pulse output from the front screen of a ION7350

Issue
A user would like to configure a KWh pulse output from the front screen of a ION7350

Product Line
ION 7350

Environment
ION 7350 Front Screen Setup

Cause 
Front panel configuration of the ION7350

Resolution
To configure the pulse outputs from the front screen or panel of an ION7350:
1. From the home screen of the ION7350 press the circle button
2. Scoll down to Adv. Meter Setup, press the circle button
3. Scroll down to Calibration Pulser Module, press the circle button
4. Select KWh exp Pulse, press the circle button
5. The following options will be available for customization:
a. CAP2 Pulse Width = This defines the width of the pulse sent from the ION meter.
b. CAP2 KT = This specifies the number of Wh's per pulse in seconds.
c. CAP2 Int Mode = Specifies the integration
d. CAP2 Output Mode = Sets the type of output
e. CAP2 Port = Rear I/O port that will send the KWh pulse

Was this helpful?
What can we do to improve the information ?