Technical FAQs

Ask a Question

PM5350 firmware update. Detailed Instructions for downloading and updating the firmware of PM5350 using DLF-3000 3.3 v2

Product Line:
PM5350
DLF-3000 

Environment:
Firmware Upgrade

Cause:
Firmware related issue.


Resolution:
*Warning: The firmware utilities listed here can cause permanent damage to your product if applied incorrectly. Before downloading any firmware updates, verify the firmware you are downloading is appropriate for the specific model number of your product. If you have any doubts, contact Technical Support for guidance. 

*Warning: Be sure all other software, is not connected to the meter.*

Use the following link to download the DLF-3000 software:
DLF-3000 Download

The attached tutorial will walk you through how to update the firmware of PM5350 meter using DLF-3000 software and serial communication:

Was this helpful?
What can we do to improve the information ?