Technical FAQs

Ask a Question

EGX300 displays readings for the 100A BCM meter incorrectly by a factor of 10

Goals and Symptoms

Symptoms
The readings on the EGX web page are 10% of the actual values for the 100A BCM model.

Facts and Changes

Environment

EGX300, 100Amp BCM models

Causes and Fixes

Cause
The EGX300 firmware was initially incorrect in that it was assumed both the 50A and 100A registers maintained the same programming. This error was corrected in the EGX300 firmware 4.3 and above.

The document for the 50A version says: "Registers 1-42 represent the real-time current for each channel (circuit) expressed in milliamps (10000 = 10.000Amps)"
The document for the 100A version says this "Registers 1-42 represent the real-time current for each channel (circuit) expressed in 10s of milliamps (1000 = 10.00 Amps)"

Resolution
The issue has been resolved with the release of firmware version 4.3 and above. Update the firmware in the EGX300 to 4.3 or greater to resolve the issue. The firmware now separates the BCM into two different devices, one for the 50A and one for the 100A model. You will need to select the correct model type and the real time current values will be corrected.


Legacy KB System (APS) Data: RESL209856 V2.0, Originally authored by MaTh on 12/04/2012, Last Edited by DaFr on 06/06/2013
Related ranges: EGX300, BCM (Branch Current Monitor)
Was this helpful?
What can we do to improve the information ?