Technical FAQs

Ask a Question

Can the ethernet option be field retrofitted on a ION7300 Series meter?

The ethernet module is a factory order option on the ION7300 series meters that cannot be added in the field. It is not a add-on card such as with the PM800 series. The meter would need to be re-ordered or returned to have the ethernet option added.


Legacy KB System (APS) Data: RESL209847 V1.0, Originally authored by MaTh on 12/04/2012, Last Edited by MaTh on 12/04/2012
Related ranges: ION7300
Was this helpful?
What can we do to improve the information ?