Technical FAQs

Ask a Question

Is it possible to change IP address of meters, gateways or communication connections in System Manager Software (SMS) for existing devices, and keep historical data intact?

How to change the IP address of a meter, gateway or communication connection in SMS:
- Take the system offline by clicking on File> Offline
- Click Setup > Communications Connection. The Setup Communications Connection dialog box displays.
- Click on the communication connection that needs to be changed, and click on Configure.
- Change the IP address for the communication connection.
- Click Ok after making the changes, and put the system back online
- Click on File>Online>System

Was this helpful?
What can we do to improve the information ?