Technical FAQs

Ask a Question

How can I determine disk usage statistics of a Windows PC?

You can determine disk usage statistics on a Windows machine with WinDirStat (Windows Directory Statistics).
WindirStat is a free, open source disk usage analyzer and cleanup tool for Microsoft Windows. The program scans disk drives and generates reports that show which directories and files are consuming the most space on the PC.

This can be useful when diagnosing hard drives that are almost full and you want to find unneeded files to delete.



WinDirStat is free software published under the GNU General Public License.

In general that means you are free to do whatever you like with the binary form (mirror it, put it on media accompanying printed magazines and also use it inside your company) free of charge.

windirstat1_1_2_setup.zipwindirstat1_1_2_setup.zip


Common questions:
How much disk space is being used?
What is taking up space on my hard drive?
Where is my space being used?


Legacy KB System (APS) Data: RESL209844 V1.0, Originally authored by MaTh on 12/04/2012, Last Edited by MaTh on 12/04/2012
Related ranges: System Manager 4.3, ION Enterprise V6.0, Power Monitoring 7.0, ION Other
Was this helpful?
What can we do to improve the information ?