Technical FAQs

Ask a Question

What is the difference between an EGX100SD and a EGX100MG?

The only difference between these two part numbers is the branding of the gateway (MG for Merlin Gerin and SD for Square D). All other physical and technical aspects are exactly the same.


Legacy KB System (APS) Data: RESL209729 V1.0, Originally authored by MaTh on 11/20/2012, Last Edited by MaTh on 11/20/2012
Related ranges: EGX100
Was this helpful?
What can we do to improve the information ?