Technical FAQs

Ask a Question

Is it possible to create a report to show daily energy usage with aggregate monthly consumption?

Goals and Symptoms

Issue
To create a report which shows daily energy usage with monthly aggregate consumption.

Facts and Changes

 

Causes and Fixes

Environment

System Manager Software (SMS) with Advanced Report, ION Enterprise (IONE) or StruxureWare Power Monitoring with Web Reporter (Reports)


Resolution

There are two reports available to display this information:

Single Device Usage Report and Multi Device Usage Report

The screen shot below shows the necessary configuration from SPM 7.


Legacy KB System (APS) Data: RESL209724 V1.0, Originally authored by MaTh on 11/20/2012, Last Edited by MaTh on 11/20/2012
Related ranges: System Manager 4.3, Power Monitoring 7.0, ION Enterprise V6.0
Was this helpful?
What can we do to improve the information ?