Technical FAQs

Ask a Question

Can the CM3/CM4/PM8's onboard logs be viewed from the ECC's webpages?

The onboard logs of the meters cannot be viewed from the ECC card, but the onboard logs may be uploaded using the latest version of ION Setup (Currently ION Setup 3.0).
Environment
CM3000, CM4000, PM800, PM8ECC, ECC21


Legacy KB System (APS) Data: RESL209658 V1.0, Originally authored by MaTh on 11/15/2012, Last Edited by MaTh on 11/15/2012
Related ranges: PM800 series, CM4000 series, CM3000 series
Was this helpful?
What can we do to improve the information ?