Technical FAQs

Ask a Question

Why are my timestamps off in Vista?

If all timestamps are off by x amount of hours, then the data is more than likely being displayed in UTC time instead of local time. To correct, go to Options -> "Show Logs in Universal Time (UTC)"
time stamps, UTC time, incorrect time or date


Legacy KB System (APS) Data: RESL209643 V1.0, Originally authored by MaTh on 11/14/2012, Last Edited by MaTh on 11/14/2012
Related ranges: Power Monitoring 7.0, ION Enterprise V6.0, ION Enterprise V5.6, ION Enterprise V5.5
Was this helpful?
What can we do to improve the information ?