Technical FAQs

Ask a Question

Netstat batch file used to find out which application is using a specific TCP port in Windows

list_tcp_ports.batlist_tcp_ports.bat
Copy the attached list_tcp_ports.bat batch file to your server and double click to run. This will create netstat_output.txt on C:\ which contains the result of the netstat -anb command in the format shown in the screen capture below.



The following articles describe issues resulting from port conflicts where the batch file from this article may be useful.
RESL192503, RESL209208, RESL191350, RESL197082


Legacy KB System (APS) Data: RESL209626 V1.0, Originally authored by AnVa on 11/12/2012, Last Edited by AnVa on 11/12/2012
Related ranges: System Manager 4.0, System Manager 4.2, System Manager 4.3, PowerLogic SCADA 7.1, PowerSCADA Expert 7.2
Was this helpful?
What can we do to improve the information ?