Technical FAQs

Ask a Question

How to read alarm status's via registers on a CM2000 series meter

The alarm status's are stored in registers 5771-5778 with each alarm set to a bit indexed from zero. For example, if one needed to determine if the over current alarm for phase A was active you would read register 5771 and look to bit zero. If the register reading program is not capable of displaying binary (bit level) information, the information may be entered into the Windows calculator and converted from decimal to binary.
Alarm No. Alarm Description
01 Over Current Phase A
02 Over Current Phase B
03 Over Current Phase C
04 Over Current Neutral
05 Over Current Ground
06 Under Current Phase A
07 Under Current Phase B
08 Under Current Phase C
09 Current Unbalance Phase A
10 Current Unbalance Phase B
11 Current Unbalance Phase C
12 Phase Loss, Current
13 Over Voltage Phase A
14 Over Voltage Phase B
15 Over Voltage Phase C
16 Over Voltage Phase A-B
17 Over Voltage Phase B-C
18 Over Voltage Phase C-A
19 Under Voltage Phase A
20 Under Voltage Phase B
21 Under Voltage Phase C
22 Under Voltage Phase A-B
23 Under Voltage Phase B-C
24 Under Voltage Phase C-A
25 Voltage Unbalance A
26 Voltage Unbalance B
27 Voltage Unbalance C
28 Voltage Unbalance A-B
29 Voltage Unbalance B-C
30 Voltage Unbalance C-A
31 Voltage Loss (Loss of A, B, or C, but not all)
32 Over kVA 3-Phase Total
33 Over KW Into the Load 3-Phase Total
34 Over KW Out of the Load 3-Phase Total
35 Over kVAR Into the Load 3-Phase Total
36 Over kVAR Out of the Load 3-Phase Total
37 Over Current Demand Phase A
38 Over Current Demand Phase B
39 Over Current Demand Phase C
40 Over Current Demand 3-phase Total
41 Over Frequency
42 Under Frequency
43 Lagging True Power Factor
44 Leading True Power Factor
45 Lagging Displacement Power Factor
46 Leading Displacement Power Factor
47 Suspended Sag/Swell
49 Over Value THD Current Phase A
50 Over Value THD Current Phase B
51 Over Value THD Current Phase C
52 Over Value THD Voltage Phase A-N
53 Over Value THD Voltage Phase B-N
54 Over Value THD Voltage Phase C-N
55 Over Value THD Voltage Phase A-B
56 Over Value THD Voltage Phase B-C
57 Over Value THD Voltage Phase C-A
58 Over K-Factor Phase A 1071 Tenths % A
59 Over K-Factor Phase B 1072 Tenths % A
60 Over K-Factor Phase C
61 Over Predicted kVA Demand
62 Over Predicted KW Demand
63 Over Predicted kVAR Demand
64 Over kVA Demand Level 1
65 Over kVA Demand Level 2
66 Over kVA Demand Level 3
67 Over kW Demand Level 1
68 Over KW Demand Level 2
69 Over KW Demand Level 3
70 Over kVAR Demand
71 Over Lagging 3-phase Avg. Power Factor
72 Under 3-Phase Total Real Power
73 Over Reverse 3-Phase Power
74 Phase Reversal
75 Status Input 1 Transition from Off to On
76 Status Input 2 Transition from Off to On
77 Status Input 3 Transition from Off to On
78 Status Input 4 Transition from Off to On
79 Status Input 5 Transition from Off to On
80 Status Input 6 Transition from Off to On
81 Status Input 7 Transition from Off to On
82 Status Input 8 Transition from Off to On
83 Status Input 1 Transition from On to Off
84 Status Input 2 Transition from On to Off
85 Status Input 3 Transition from On to Off
86 Status Input 4 Transition from On to Off
87 Status Input 5 Transition from On to Off
88 Status Input 6 Transition from On to Off
89 Status Input 7 Transition from On to Off
90 Status Input 8 Transition from On to Off
99 End of Incremental Energy Interval
100 Power-Up/Reset
101 End of Demand Interval
102 End of Update Cycle
103 Over Analog Input Channel 1
104 Over Analog Input Channel 2
105 Over Analog Input Channel 3
106 Over Analog Input Channel 4
107 Under Analog Input Channel 1
108 Under Analog Input Channel 2
109 Under Analog Input Channel 3
110 Under Analog Input Channel 4
201 Voltage Swell A-N/A-B
202 Voltage Swell B-N
203 Voltage Swell C-N/C-B
204 Current Swell Phase A
205 Current Swell Phase B
206 Current Swell Phase C
207 Current Swell Neutral
208 Voltage Sag A-N/A-B
209 Voltage Sag B-N
210 Voltage Sag C-N/C-B
211 Current Sag Phase A
212 Current Sag Phase B
213 Current Sag Phase C
214 Current Sag Neutral


Legacy KB System (APS) Data: RESL209554 V1.0, Originally authored by MaTh on 11/02/2012, Last Edited by MaTh on 11/02/2012
Related ranges: CM2000 series
Was this helpful?
What can we do to improve the information ?