Technical FAQs

Ask a Question

Is the configuration of an ECC card stored in the meter or in the card itself?

The configuration of the ECC (IP address, subnet mask, default gateway) is stored in the meter itself. If an existing meter with an ECC is replaced but still uses the original ethernet card, then the configuration will have to be set again in the new meter.
Environment
PM800, PM8ECC, CM3000, CM4000, ECC21


Legacy KB System (APS) Data: RESL209545 V1.0, Originally authored by MaTh on 11/01/2012, Last Edited by MaTh on 11/01/2012
Related ranges: CM4000 series, CM3000 series, PM800 series, PM8ECC, ECC21
Was this helpful?
What can we do to improve the information ?