Technical FAQs

Ask a Question

Micrologic 5.2x, 5.3x, 6.2x, and 6.3x user guide

The trip units described in this manual:
Micrologic 5.2 A, 5.3 A, 5.2 E and 5.3 E trip units
Micrologic 6.2 A, 6.3 A, 6.2 E and 6.3 E trip units
Micrologic 6.2 E-M and 6.3 E-M trip units


Compact NSX Micrologic 5/6

micrologic_5_6_2.pdf


Legacy KB System (APS) Data: RESL209513 V2.0, Originally authored by MaTh on 10/27/2012, Last Edited by MaTh on 11/01/2012
Related ranges: Communication with Micrologic trip units
Was this helpful?
What can we do to improve the information ?