Technical FAQs

Ask a Question

Does the ION6200 support high-leg delta wiring?

Does the ION6200 series meter support 4-wire high leg delta.

Product Line

Meter Wiring

Meter installation guide does not show a 4-wire high leg delta. 

Yes, the ION6200 can be wired to monitor a 4-wire high leg delta. The 4-wire wye volts mode should be used and the wiring diagram would be the same as 4-wire wye.

With 4-wire high leg delta, there are some measured quantities that will be incorrect or invalid such as Voltage line to neutral average (VLN Average) and Voltage line to line average (VLL Average).
For a complete list of incorrect or invalid quantities, see the attached document. 
Was this helpful?
What can we do to improve the information ?