Technical FAQs

Ask a Question

Why do numeric objects for my custom diagrams point to the same device for each meter?

This is most likely occurring because the Link is set to "Custom" instead of "Inherit from parent window"


Legacy KB System (APS) Data: RESL209366 V1.0, Originally authored by MaTh on 10/10/2012, Last Edited by MaTh on 10/10/2012
Related ranges: Power Monitoring 7.0, ION Enterprise V6.0, ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?