Technical FAQs

Ask a Question

Using the Modbus Tester Interface within ION Setup 3.0

Product Line
ION Setup

Environment
Modbus Tester Interface

Resolution
When communicating with Modbus protocol, ION Setup has an interface that can be used as Modbus Tester to read/write registers. When connecting to PowerLogic Circuit Monitors such as CM3000 or CM4000, this feature becomes handy to read/write registers which are not already in the default screens. Note that this is not limited to device types that are supported by default, but also for third party devices in which a communication can be established.

Procedure
It is assumed the communication connection is already setup in ION Setup (in Network mode a 'site' and 'device' are created). Follow the steps below:

  1. On the tool bar click on the stethoscope to open diagnostic window ; or from the menu select Tools > Diagnostics...
  2. Go to 'Troubleshooting' tab and open the 'Modbus Tester Interface'.
  3. From the drop down menu select the proper option for your application; for the sake of this demonstration 'Read Holding Registers (0x03)' is selected.


  1. Input the required parameters and click 'Send'; in this example register 41716, Total Real Energy, which is type Mod10 and size of 4 is used:


Modbus Request Type

The three available selections are:

  1. "Single Read"
  2. "Polled Read"; the user is prompted for polling rate:


  1. "Polled Read & Log"; as the name implies this feature has the capability to log the data. Below is an example of the output file:


Write to Register

Two options available:

  1. Preset "Single" Register (0x06)
  2. Preset "MultipleRegisters (0x10)





After selection and assigning the address, highlight the register and enter the value to write by clicking on 'Set...' and then 'Send':

Note: ION Setup version 3.0.12242.01 was used when this articles was written.
Was this helpful?
What can we do to improve the information ?