Technical FAQs

Ask a Question

Can I reconfigure the ION8600 I/O module analog outputs from 0-20 mA to -1 to 1 mA?

It is not possible to configure the outputs from -1 to +1 in the field. The analog outputs on the I/O expander can change to either 0-20mA or 4-20mA however.


Legacy KB System (APS) Data: RESL209283 V1.0, Originally authored by MaTh on 10/04/2012, Last Edited by MaTh on 10/04/2012
Related ranges: ION8600
Was this helpful?
What can we do to improve the information ?