Technical FAQs

Ask a Question

What is the UL File Number for ION6200, ION73XX, ION7X00, and ION7X50?

Issue
Where can the UL file number for an ION meter be found?

Product Line
ION6200, ION73XX, ION7X00, ION7X50

Environment
UL File Number

Resolution
The UL file number is PICQ.E189364, which covers multiple product lines: ION6200, ION73XX, ION7X00, ION7X50, etc.
For more information regarding UL, see the following link here.

**Note: This link will take you to an external site not controlled by Schneider Electric**

If this link has changed or other Schneider UL documents are required, try searching on the UL website with Company Name and Keyword: 
http://database.ul.com/cgi-bin/XYV/template/LISEXT/1FRAME/index.html

Was this helpful?
What can we do to improve the information ?