Technical FAQs

Ask a Question

How many remote device connections are available on the EGX300?

The EGX300 can open connections for up to 16 unique, user-defined remote Modbus TCP/IP devices.


Legacy KB System (APS) Data: RESL209200 V2.0, Originally authored by MaTh on 09/26/2012, Last Edited by MaTh on 11/01/2012
Related ranges: EGX300
Was this helpful?
What can we do to improve the information ?