Technical FAQs

Ask a Question

Is ION Setup capable of sending emails?

Can ION Setup send an email

Product Line
ION Setup

Software Capabilities

ION Setup is only intended to configure meters and pull onboard information for certain meters with that functionality. If a customer is wanting a way to email or alert based on power quality events then they will require either the Struxureware Power Monitoring software or an ION meter with the Alert Module feature.

Was this helpful?
What can we do to improve the information ?