Technical FAQs

Ask a Question

Event Notification Module 7.0 (ENM) Documentation (Installation Guide, User Guide, Brochure/Handout)

Attached is the included documentation for ENM 7.0 (ENM 7), and the ENM brochure.
SQL Express Install Guide.pdfENMUserGuide.pdfENM Installation Guide.pdfENM_Handout.pdfENM_Handout.pdf


Legacy KB System (APS) Data: RESL209157 V2.0, Originally authored by MaTh on 09/20/2012, Last Edited by DaFr on 06/21/2013
Related ranges: SMS Add-on, Paging Module
Was this helpful?
What can we do to improve the information ?