Technical FAQs

Ask a Question

Does changing the options card for the ION6200 reset the meter settings?

Although changing the options card does involve removing the power supply from the unit, it does not reset the configuration settings such as the PT/CT ratios and volts mode.


Legacy KB System (APS) Data: RESL209048 V1.0, Originally authored by MaTh on 09/11/2012, Last Edited by MaTh on 09/11/2012
Related ranges: ION6200
Was this helpful?
What can we do to improve the information ?